Use the Archive Settings Manager to archive events, trend logs, and extended trend logs on the Enterprise Server or Enterprise Central.
Number |
Description |
Enabled |
Select to activate the archiving function on the Enterprise Server or Enterprise Central. For more information, see Enabling the Archiving Function and Defining the Archive Folder . |
Disabled |
Select to disable the archiving function on the Enterprise Server or Enterprise Central. |
Archive Now |
Click to archive the selected historical data immediately. For more information, see Manually Creating an Archive . |
Alarm Events |
Select to include Alarm events in the archive. |
User Events |
Select to include User events in the archive. |
System Events |
Select to include System events in the archive. |
![]() |
Click to add an extended trend log to the list. |
![]() |
Click to delete an extended trend log from the list. |
Extended Trend Log |
Select the logs that you want to include in the archive. |
Archive Schedule |
Click Schedule to configure a schedule for archiving. For more information, see Manual and Scheduled Archiving . |
Output Type |
Select an output type for the archive. For more information, see Archive Formats and Storage . |
Path |
Type the path to the location where you want store the archive files. For more information, see Enabling the Archiving Function and Defining the Archive Folder . |
Validate |
Click to validate that the path is valid. A green checkmark ![]() |