Actions Menu – Actions Submenu

Use the Actions submenu to create manual archives from an Enterprise Server or an Enterprise Central.

 
action_zoom_plus_stroke Actions Menu – Actions submenu

Actions Menu – Actions submenu

Table: Actions Menu – Actions Submenu

Command

Description

Create archive(s) now

Creates a manual archive that is saved to a predefined path on the computer running WorkStation. For more information, see Archive Settings Manager Dialog Box .

  • Manual and Scheduled Archiving
  • Archive Settings Manager Dialog Box
  • Manually Creating an Archive