Displaying Property Bindings in a Search Result

You display property bindings in a search result when you want to check that you have bound correctly.

Note:

You use search to display in-bound properties.

To display property bindings in a search result
  1. In WorkStation, on the WorkStation Toolbar, click the Search button

     
    action_zoom_plus_stroke
    .

  2. In the Search view, in the Object name box, enter the name of the object to search for.

  3. In the In folder box, enter the path to the folder or container object you want to search.

  4. Select Search for properties .

  5. Enter a property name.

  6. In the Include types box, enter the type you want to search for if you want to narrow the search to specific object types.

  7. Click the Search icon

     
    action_zoom_plus_stroke
    .

  8. In the search result List View, right-click the column heading row and then click Add/Remove columns .

  9. In the Add/Remove Columns dialog box, select Property binding .

  10. Click OK .

  • Search
  • Search View
  • Bindings Overview
  • WorkStation Toolbar
  • Add/Remove Columns Dialog Box (Search)