earth_america
user_standard Log on
action_search_stroke
earth_america
Log on to rate and give feedback 1 2 3 4 5 Log on to rate
0
User Interface

User Interface


Products: SpaceLogic Sensor
Functionalities: Hardware, Touchscreen
Product version: 3.3, 2022
7/23/2021

SpaceLogic Sensor Touchscreen Display Model- Functions Menu Screen

Use the SpaceLogic Sensor Touchscreen Display model functions menu to perform a variety of tasks. For example, with the functions menu configured as shown, you can perform the following tasks:

  • Change occupancy

  • Change fan speed

  • Change the degree type

  • Change heating or cooling mode

  • Adjust the temperature setpoint

  • Control the lights

  • Control the blinds

  • Configure scenes

 
action_zoom_plus_stroke SpaceLogic Sensor Touchscreen Display model- functions menu screen

SpaceLogic Sensor Touchscreen Display model- functions menu screen

Table: SpaceLogic Sensor Touchscreen Display Model- Functions Menu Screen

Button

Description

 
action_zoom_plus_stroke

Click to return to the front menu screen.

 
action_zoom_plus_stroke

Click to change the occupancy mode. For more information, see Changing the Occupancy Mode .

 
action_zoom_plus_stroke

Click to access the fan speed menu where you can toggle to the desired fan state. For more information, see Selecting the Fan Speed .

 
action_zoom_plus_stroke

Click to switch the degree type from Fahrenheit to Celsius or Celsius to Fahrenheit. For more information, see Selecting the Degree Type .

 
action_zoom_plus_stroke

Click to access the heating and cooling menu, where you can toggle to the available choices: heating, cooling, or automatic. For more information, see Changing the Heating and Cooling Mode .

 
action_zoom_plus_stroke

Click this button to adjust the temperature setpoint. For more information, see Changing the Temperature Setpoint .

 
action_zoom_plus_stroke

Click this button to turn the lights on or off, or dim the lights.

For more information, see Turning the Lights On and Off .

For more information, see Dimming the Lights .

 
action_zoom_plus_stroke

Click this button to fully open and close the blinds or incrementally adjust the blinds.

For more information, see Fully Opening and Closing the Blinds .

For more information, see Incrementally Adjusting the Blinds .

 
action_zoom_plus_stroke

Click this button to access the scenes menu. For more information, see Selecting the Scenes Menu .

  • SpaceLogic Sensor Touchscreen Display Model
  • Changing the Temperature Setpoint
  • Selecting the Fan Speed
  • Selecting the Degree Type
  • Changing the Occupancy Mode
  • Changing the Heating and Cooling Mode
  • Turning the Lights On and Off
  • Dimming the Lights
  • Fully Opening and Closing the Blinds
  • Incrementally Adjusting the Blinds
  • Selecting the Scenes Menu