Use this workflow to add licenses to automation servers with access to Internet using Device Administrator.
Related information can be found in the sections after the flowchart.
action_zoom_plus_stroke
Automation Server licensing workflow
Install certificates on the Automation Servers
Install certificates if you use HTTPS for communication.
For more information, see Device Administrator Certificate Workflow
.
Make sure that the Automation Servers have access to Internet
The Automation servers must have access to Internet for the activation process.
Add Entitlements to Device Administrator
In Device Administrator, add an Entitlement that contains products and licenses to Device Administrator.
For more information, see Adding an Entitlement to Device Administrator
.
Assign licenses to an automation server
Assign the licenses in the Entitlement for the features you want to use on the automation servers.
For more information, see Assigning Licenses
.
Activate licenses on an automation server
For more information, see Activating Licenses Online
.
Important:
Activated licenses cannot be deactivated.