The RP controller expansion modules provide a range of devices that can be combined to form a connected room solution. The RP controller expansion modules are connected to the RP-C room bus and provide the RP-C room controllers with I/O expansion and sensors that enable lighting and blind control.
The software application for lighting and blind control runs in the RP-C controller. There is typically one RP-C controller per room, but some RP-C controller models support control of up to four rooms per controller. For more information, see RP-C Models .. The RP-C controllers are connected to an automation server, which controls and manages all the RP-C controllers. There is typically one automation server per floor. The automation servers are in turn typically connected to an Enterprise Server.
The RP-C controllers can use input data from SpaceLogic Sensor devices to control the lighting and blinds. The SpaceLogic Sensor devices are connected to the RP-C sensor bus. The SpaceLogic Sensor devices provide sensors for temperature, humidity, CO 2 , and occupancy in a room. SpaceLogic Sensor models with touchscreen display enable users to adjust the lighting and blinds in a room. For more information, see SpaceLogic Sensors - SXWS Sensors for MP and RP IP Controllers - Specification Sheet .
In addition, the EcoStruxure Building Engage mobile application allows building occupants to adjust the room comfort settings (room temperature, fan speed, lighting, and window blinds) using a smartphone connected to the RP-C controller through Bluetooth Low Energy. For more information, see Engage .
The RP controller expansion light modules enable control of lights with electrical ballasts and LED drivers.
For more information, see Light Modules .
The RP controller expansion blind modules enable control of motorized window blinds and shutters.
For more information, see Blind Modules .
The RP controller expansion relay modules enable control of lights and motorized window blinds and shutters.
For more information, see Relay Modules .
The RP controller expansion sensor modules can be used, for example, for infrared motion detection and luminosity measurement.
For more information, see Sensor Modules .
The RP-C-RC-BLE remote control connects wirelessly to the RP controller expansion sensor module, such as the Multi-sensor and Insight-Sensor, and enables the occupants of modern office buildings to control the comfort level of their space.
For more information, see RP-C-RC-BLE .