earth_america
user_standard Log on
action_search_stroke
earth_america
Log on to rate and give feedback 1 2 3 4 5 Log on to rate
0
How to

How to


Products: WebStation
Functionalities: Schedules
Product version: 2022
12/17/2021

Removing a Schedule from a Multi Schedule Viewer

You remove unused schedules from a Multi schedule viewer.

Show More
action_close

You can create a Multi schedule viewer in WebStation to edit and view a number of schedules at the same time.

A Multi schedule viewer is useful for example if you want to add at the same events on several schedules at the same time. You can select the schedules you want to add the events on.

A Multi schedule viewer also gives you an overview of the attached schedules.

To remove a schedule from a Multi schedule viewer
  1. In WebStation, click the Multi schedule viewer.

  2. Select the schedule you want to remove.

  3. Click the Remove selected schedule button

     
    action_zoom_plus_stroke
    .

  4. Click Save .

  • Multi Schedule Viewer
  • Multi Schedule Viewer Workspace
  • Multi Schedule Viewer Toolbar
  • Creating a Multi Schedule Viewer
  • Adding a Schedule to a Multi Schedule Viewer
  • Adding the Same Event to Multiple Schedules
  • Assigning a Value on Click
  • Opening a Schedule from a Multi Schedule Viewer