earth_america
user_standard Log on
action_search_stroke
earth_america
Log on to rate and give feedback 1 2 3 4 5 Log on to rate
0
Concept

Concept


Products: AS-B, Enterprise Central, Enterprise Server, AS-P
Functionalities: Semantic
Product version: 2022
8/31/2022

Semantic Overview

arrow1_rotationSPARQL Database arrow1_rotationOntologies arrow1_rotationSemantic Data and EWS arrow1_rotationLicensing arrow1_rotationSemantic Navigation arrow1_rotationConfigure ExoStruxure Building Automation System to use Semantic Tagging arrow1_rotationSemantic Engineering

The ExoStruxure Building Operation software supports a database solution for external storage of semantic information.

The semantic information is a contextual representation of a building that follows the Brick schema. It includes representation of building assets such as points, locations, and equipment.

The semantic information is configured in WorkStation, and the information is available in WorkStation and WebStation. The information is also available through EcoStruxure Web Services.

A stand-alone automation server does not support sematic tagging.

SPARQL Database

EcoStruxure Building Operation uses a Sparql database, GraphDB from Ontotext, to handle semantic queries.

For more information, see Sparql Database .

Ontologies

Semantic is based on ontologies.

For more information, see Ontologies .

Semantic Data and EWS

The EWS metadata makes it possible to add semantic information to the EWS items, provided that the EBO object that is exposed by EWS is semantically described.

Semantic tagging is exposed using EWS.

For more information, see Semantic Data and EWS .

Licensing

You can use a limited number of queries in the Graph database without a license. To be able to use the Graph database to its full extent a license is needed.

If you use an GraphDB on another location than the EBO default location, you have to aquire a license.

Semantic Navigation

You can navigate the semantic database using search and filter.

For more information, see Semantic Navigation in WorkStation .

Configure ExoStruxure Building Automation System to use Semantic Tagging

Use this workflow to configure EcoStruxure Building Automation system to use semantics.

For more information, see Configure EcoStruxure Building Automation System to use Semantic Workflow .

Semantic Engineering

Semantic engineering is the process describing an EcoStruxure Building operation database using semantic s .

For more information, see Semantic Engineering Overview .

  • Semantic Navigation in WorkStation
  • Sparql Database
  • Ontologies
  • Semantic Data and EWS
  • Configure EcoStruxure Building Automation System to use Semantic Workflow
  • Semantic Engineering Overview