Use this workflow to configure EcoStruxure Building Automation system to use semantics.
For security reasons, change the password for the admin user on the Spargl database. Changing the password on the admin user on Sparql database helps to protect the Sparql database. If the password is not changed the EBO generates a system alarm.
The password for the Admin user on the Ontotext GraphDB Sparql database is "root".
For more information, see Navigating to the Sparql Database .
Refer to the Sparql database documentation.
In a default set up you normally do not have to do any changes in the configuration. Changes in the configuration are only done if you want to change the EBO user that connects to the Sparql database, use a Sparql database on another location than the default location, or change or rename the repository.
For more information, see Configuring the Semantic Settings .
Users in EcoStruxure Building Operation must be allowed to use semantics. This is done on user group level. The group Admin are by default allowed to use semantics.
For more information, see Configuring Semantic Permissions .