You configure the semantic settings if you, for example, want to change the EBO user that connects to the Sparql database or use a Sparql database on another location than the default location.
In WorkStation, in the System Tree pane, select the EBO server.
Click the Control Panel tab.
Click Settings .
Configure the settings.
Component |
Description |
SPARQL DB URL |
Enter the address to the Sparql database. |
Repository |
Type the name to the repository on the Sparql database you want to use. |
Username |
Enter the username of the EBO user that you want to use to connect with the Sparql database. |
Password |
Type the password of the EBO user that you want to use to connect to the Sparql database.
|
Confirm password |
Confirm the password for the EBO user. |
Query Timeout |
Enter the timeout the EBO server uses for normal queries against the Sparql database. |
Update Timeout |
Enter the timeout the EBO server uses for uploading ontologies to Sparql database. |
Search Timeout |
Enter the timeout the EBO server uses for search queries against the Sparql database. |
Export Timeout |
Enter the timeout the EBO server uses for export queries against the Sparql database. |
Insert Batch Size |
Enter the maximum batch size of files imported to the EBO server from the Sparql database. |
Lead object |
The lead-shadow mechanism is automatically configured for the Sparql database in all EBO servers in the system. You should not change this if you use the same Sparql database for the whole EBO system.
|
Click OK .