earth_america
user_standard Log on
action_search_stroke
earth_america
Log on to rate and give feedback 1 2 3 4 5 Log on to rate
0
How to

How to


Products: Commission, IP-IO , MP-C, MP-V, RP-C
Functionalities: Engineering, BACnet/IP devices
Product version: 2022
7/21/2022

Logging on to the Commission Mobile Application

You log on to the Commission mobile application to perform commissioning, flow balance, and checkout operations on BACnet/IP controllers.

Show More
action_close

The Commission mobile application allows you to use a mobile device to perform commissioning, flow balance, and checkout operations on SpaceLogic BACnet/IP devices. BACnet/IP devices include BACnet/IP controllers (MP and RP), and IP-IO modules. The Commission mobile application is available for Android and iOS (Apple) phones and tablets, as well as devices using Microsoft Windows 10. The Commission mobile application can connect to a single BACnet/IP device or to a network of BACnet/IP devices on the local network.

Device Connection

The Commission mobile application supports device connection through BACnet Wi-Fi and wireless Bluetooth connection.

For more information, see Device Connection .

Bluetooth Adapter

The SpaceLogic Bluetooth Adapter allows you to establish a Bluetooth connection to MP controllers. You plug the Bluetooth Adapter into the corresponding SpaceLogic Sensor to connect to the controller.

For more information, see SpaceLogic Bluetooth Adapter .

Device Configuration

You download an image to a BACnet/IP controller to facilitate device commissioning tasks and then use the Device Settings view to configure the settings of the BACnet/IP controller.

For more information, see BACnet/IP Controller Device Settings .

Configuration Menu

Configuration Menus are a group of pre-engineered objects and values that make device commissioning faster and easier. Configuration Menus are exported and downloaded from image files. Download a Configuration Menu to a BACnet/IP controller to commission the controller.

For more information, see Configuration Menu .

I/O Checkout

After you have wired the physical inputs and outputs of the controller, you perform I/O checkout to verify that the wiring was done correctly and that the physical inputs and outputs are working properly.

For more information, see I/O Checkout Overview .

Flow Balancing

The Flow Balance function of the Commission mobile application is used to air balance terminal boxes controlled by MP-V controllers. This function automates most of the air balance procedure but it also allows you to manually check out the flow balance by driving the damper to a specified position, a flow setpoint, or a flow value.

For more information, see Flow Balancing .

Device Restart

Use the Device Restart function of the Commission mobile application to perform a restart of the BACnet/IP controller. There are four different ways to restart the BACnet/IP controller.

For more information, see Device Restart .

To log on to the Commission mobile application
  1. Download and then install the Commission mobile application to the mobile device or Windows 10 laptop from Google Play, the Apple App Store, or the Microsoft Store.

    Tip:

    EcoStruxure Building Commission is the name of the application used in the download sources.

  2. From your mobile device or Windows 10 laptop, launch the application by logging on with your Schneider Electric extranet credentials while connected to the internet.

    Important:

    You can now use the mobile application for 90 days without an internet connection. During this period, you can close and launch the mobile application without logging in. If you log out, an internet connection is required to log in again. Seven days prior to the expiration of the 90 day period, you will start receiving messages to remind you to log in while connected to the internet to start a new 90 day period.

    A page then displays with the name of the product, EcoStruxure Building Commission. It is followed by a prompt indicating that By using this product, you accept its Terms of Use .

  3. Click Terms of Use to view and scroll through the Terms of Use pages

  4. Export this information if you wish by clicking the button on the right side of the page.

    The information is then exported elsewhere on your device

  5. Click Close to exit the Terms of Use page and then click Accept and Continue .

    You will not see that Terms of Use prompt next time you log in.

    The logon page displays next and includes the product name and application software version.

  6. Click Log on .

    The logon process has been integrated with Schneider Electric’s identity management system.

  7. On the ensuing EcoStruxure Building Commission page, enter your email address and click Next or click the single sign-on button

     
    action_zoom_plus_stroke
    to continue with your Schneider Electric Exchange account.

    If you do not have a user account, click Register here to register here as a new user and create one.

    Once you have authenticated your user account, the Consent Management page displays and you are prompted to Personalize Your Experience .

  8. Please opt in to allow Schneider Electric to utilize your real-world use case data to improve the mobile application in the future.

    Tip:

    Should you opt in, you can change permission settings at any time by accessing the Consent Management page from the More menu. For more information, see Accessing and Using the More Menu .

  9. Click the button

     
    action_zoom_plus_stroke
    to turn on and send analytic events based upon what you are doing in the application.

    If you click to turn it off, you do not send any analytic data.

  10. Click Close to exit and bring up the familiar Connect page.

    From now on, when you launch the Commission mobile application from your mobile device, you will immediately come to the Connect page. You no longer need to perform the user authentication process unless you logout.

  • Commission Mobile Application
  • Accessing and Using the More Menu