earth_america
user_standard Log on
action_search_stroke
earth_america
Log on to rate and give feedback 1 2 3 4 5 Log on to rate
1
Concept

Concept


Products: Commission, IP-IO , MP-C, MP-V, RP-C
Functionalities: Engineering, BACnet/IP devices
Product version: 2022
12/17/2021

Configuration Menu

Configuration Menus are a group of pre-engineered objects and values that make device commissioning faster and easier. Configuration Menus are exported and downloaded from image files. Download a Configuration Menu to a BACnet/IP controller to commission the controller.

Configure Controllers Workflow

You download an Application Image that contains a Configuration Menu to a BACnet/IP controller to configure a device. Use this workflow to implement the Configuration Menu using the Commission mobile application. Related information can be found in the section after the flowchart.

For more information, see Configure Controllers with the Configuration Menu Workflow .

Download a Configuration Menu to a BACnet/IP Controller

You download the Configuration Menu to the BACnet/IP controller to configure the device.

For more information, see Downloading a Configuration Menu to a BACnet/IP Controller .

Modify Device Properties from the Configuration Menu

After downloading the configuration menu to the controller, you view and modify the device properties from the configuration menu to complete device commissioning.

For more information, see Modifying Device Properties from the Configuration Menu .

  • Commission Mobile Application Overview
  • Configure Controllers with the Configuration Menu Workflow
  • Downloading a Configuration Menu to a BACnet/IP Controller
  • Modifying Device Properties from the Configuration Menu