You download an Application Image that contains a Configuration Menu to a BACnet/IP controller to configure a device. Use this workflow to implement the Configuration Menu using the Commission mobile application. Related information can be found in the section after the flowchart.
Configure controllers with the Commission mobile application workflow
Transfer the Application Image to your mobile device or Windows 10 laptop.
For more information, see Transferring an Application Image File .
In the Commission mobile application, connect to the controller.
For more information, see Connecting to a Device through WiFi .
For more information, see Connecting to a Controller through Bluetooth .
Download the Application Image to the BACnet/IP controller.
For more information, see Downloading an Image File to a BACnet/IP Controller .
Download the Configuration Menu to the BACnet/IP controller.
For more information, see Downloading a Configuration Menu to a BACnet/IP Controller .
View the property values and modify them if needed.
For more information, see Modifying Device Properties from the Configuration Menu .