Product version: 2022
7/5/2022

Backup and Restore using WebStation

A subset of backup and restore features are available in WebStation.

You can create backups of the server using WebStation. The backup can be downloaded from the server.

The server can be restored using backups on the server, but you cannot upload a backup to the server. Uploading backups must be done using WorkStation.

Scheduled backup and restoring downloaded backups must be done using WorkStation.

For more information, see Backup .

  • Backup and Restore Overview
  • Backing up and Restoring using WebStation
  • Backup