Product version: 2022
7/5/2022

Backing up and Restoring using WebStation

You can backup and restore the server from WebStation. You can also download a backup.

Show More
action_close

A subset of backup and restore features are available in WebStation.

You can create backups of the server using WebStation. The backup can be downloaded from the server.

The server can be restored using backups on the server, but you cannot upload a backup to the server. Uploading backups must be done using WorkStation.

Scheduled backup and restoring downloaded backups must be done using WorkStation.

For more information, see Backup .

To backup and restore
  1. Click WebStation, click Workspace menu .

  2. Click System .

  3. Click Backup and restore .

  4. In the Backup and restore dialog:

    • Click Backup to create a manually initiated backup.

    • Select a backup and click Restore to restore the server to the selected backup.

    • Select a backup and click Download to download the selected backup.

  • Backup and Restore Overview
  • Backing up and Restoring using WebStation
  • Backup