666 Topic(s)
EcoStruxure Building Management is an integration platform for monitoring, control, and management of energy, lighting, fire safety, security and HVAC.
You backup your EcoStruxure BMS server data so that it can be restored after damage or loss due to hardware or software failures, security threats, or application testing.
There are a number of differences in functionality between WebStation and WorkStation.
An alarm pie chart is a circular graphic divided into slices to illustrate proportions of alarms.
An alarm count displays the number of alarms from the EcoStruxure Building Operation system.
Use the Workspace tab to select workspace, access help, or log off.
Use the Default Regional Settings dialog box to adapt WebStation to your region.
A subset of backup and restore features are available in WebStation.