41 Topic(s)
Values in Building Operation are stored in the Building Operation database with all input decimals. If a stored value consists of more decimals than the operating system is defined to display, the value is rounded off according to the operating system settings before it is displayed in WorkStation.
To adjust the SmartStruxure server device time, time zone, and DST, you have to access the SmartStruxure server device through a WorkStation.
You manually adjust the SmartStruxure server device clock when you configure or commission a SmartStruxure server device. When the SmartStruxure server device is running on a fully commissioned site it is important that you use a network time server to avoid drifting time in the SmartStruxure server device.
Use the Basic tab to configure the properties of the Time zone object.
You can configure the time and date on your SmartStruxure server devices using WebStation. WebStation cannot be used to configure time and date on an Enterprise Server.
In WorkStation, all times are by default displayed in local time. This means that a time, independent of its source, is displayed in the same time zone as the operating system on which WorkStation is installed. By configuring the operating system time and time zone settings, you configure how times are displayed in WorkStation. For more information, please refer to the manufacturer’s manual for the operating system.
Consistent date and timestamping across a network is critical for system wide access control, security, communications, scheduling, alarms, and events. Network time uses the NTP protocol that provides the correct current UTC time.
WorkStation supports the metric prefix range from yocta (10-24) to yotta (1024). The use of a prefix is optional and is defined together with the unit.
Use the Basic tab to configure the properties of the Time object.
Use the Time and Date editor to configure the network time server addresses or configure time on SmartStruxure servers.