earth_america
user_standard Log on
action_search_stroke
earth_america
Log on to rate and give feedback 1 2 3 4 5 Log on to rate
0
How to

How to


Products: Automation Server, AS-B, AS-P, Project Configuration Tool
Functionalities: Localization
Product version: 1.9
9/11/2019

Manually Changing the SmartStruxure Server Device Time and Date

You manually adjust the SmartStruxure server device clock when you configure or commission a SmartStruxure server device. When the SmartStruxure server device is running on a fully commissioned site it is important that you use a network time server to avoid drifting time in the SmartStruxure server device.

Note:
  • The Date & Time view displays the local time in the perspective of the SmartStruxure server device time zone settings and not in the perspective of WorkStation.

Show More
action_close

​To adjust the SmartStruxure server device time, time zone, and DST, you have to access the SmartStruxure server device through a WorkStation.

When adjusting the SmartStruxure server device clock, you can either set the time manually or you can refer to a network time server that automatically synchronizes the clock. Manual adjusting is used when you configure or commission a SmartStruxure server device. When the SmartStruxure server device is running on a fully commissioned site, it is important that you use a network time server to avoid drifting time in the SmartStruxure server device.

When adjusting the SmartStruxure server device time through WorkStation, it is the SmartStruxure server device operating system clock you adjust. Building Operation has a transparent layer above the SmartStruxure server device operating system which manages the information about the time zone and DST time offset.

 
action_zoom_plus_stroke  The Automation Server uses the operating system clock to which Building Operation adds the time zone offset and DST

The Automation Server uses the operating system clock to which Building Operation adds the time zone offset and DST

Instead of configuring the time of each SmartStruxure server device, you can create a lead and shadow relationship that makes it possible to configure several SmartStruxure server devices through a single Enterprise Server.

To manually change the SmartStruxure server device time and date
  1. ​On the Tools menu, click Control Panel .

  2. On the Control Panel toolbar, select the SmartStruxure server device.

     
    action_zoom_plus_stroke
  3. ​Click Network time and time zones .

  4. In the SmartStruxure server device Date & time view, select Manually adjust date & time .

     
    action_zoom_plus_stroke
  5. In the Local date & time boxes, enter the date and time of the SmartStruxure server device.

  6. Click the Save button

     
    action_zoom_plus_stroke
    .

  • Network Time
  • Time and Time Zone Configuration in Automation Server
  • SmartStruxure Server Device – Date & Time View
  • Synchronizing the SmartStruxure Server Device Clock
  • Changing the Time Zone of a SmartStruxure Server
  • Creating a Custom Time Zone of a SmartStruxure Server