earth_america
user_standard Log on
action_search_stroke
earth_america
Log on to rate and give feedback 1 2 3 4 5 Log on to rate
0
Concept

Concept


Products: Automation Server, AS-B, Enterprise Server, AS-P, Project Configuration Tool
Functionalities: Localization
Product version: 1.9
10/12/2017

Network Time

​Consistent date and timestamping across a network is critical for system wide access control, security, communications, scheduling, alarms, and events. Network time uses the NTP protocol that provides the correct current UTC time.

Network Time on WorkStation and Enterprise Server

The network time settings on WorkStation and Enterprise Server are configured through the operating system settings on which WorkStation or Enterprise Server is installed. For more information on how to configure network time settings, refer to the manufacturer’s manual for the operating system.

Network Time Server on a SmartStruxure Server Device

To configure SmartStruxer server device network time settings, you have to log on to the SmartStruxure server device through WorkStation. When logged in, the SmartStruxure server device has a Date & Time view where you configure the network time server addresses.

When configuring the SmartStruxure server device network time server address, you can define two time server addresses: primary time server and secondary time server. If the SmartStruxure server device fails to connect to the primary time server, it tries to synchronize its clock with the secondary.

Authenticated Network Time Servers

To increase the security of your system, you can use authenticated network time. By using authenticated network time, you decrease the risk that someone will tamper with your time setting.

To be able to use authenticated network time, you connect your SmartStruxure server to an authenticated time server. You need the secure key ID and and key value password that is provided by the authenticated time server administrator.

You can use the lead/shadow relationship to transfer the authenticated time server setting and its secure key ID and key value password from the lead server or you can configure the secure time server manually on your SmartStruxure server. When you use the lead/shadow relationship the Enterprise Server transfers the setting for the time server to the SmartStruxure server device. The SmartStruxure server device then uses the authenticated time server configuration to go online and get the correct time from the secure time server.

 
action_zoom_plus_stroke The lead and shadow relationship.  

The lead and shadow relationship.  

  • Time and Time Zone
  • Regional and Language Overview
  • SmartStruxure Server Device – Date & Time View
  • Synchronizing the SmartStruxure Server Device Clock
  • Synchronizing Time Zone Settings on Multiple SmartStruxure Server Devices