268 Topic(s)
The External Log Storage feature uses an external database administered by a combination of TimescaleDB and PostgreSQL software. The EcoStruxure Building Operation backup and restore feature cannot be used to back up and restore the External Log Storage data. Instead you use the backup and restore function of TimescaleDB. See the TimescaleDB documentation for instructions.
You disable the TimescaleDB connection for all servers that are supposed to have a connection to the database you are backing up and/or restoring to make sure you are working with the correct database.
You enable the TimescaleDB connection for all servers that are supposed to have a connection to the database you are backing up and/or restoring to make sure you are working with the correct database.
You create a log processing trend log to enable calculation within or between various trend logs.
Use the Log Processing Trend Log - Basic tab to create a log processing trend log to enable calculation within or between various trend logs.
You create a log when you want to track changes of an object.
You use trend logs to record values, such as a sensor. A trend log can also log consumptions, such as energy consumption or water consumption.
A trend log is a collection of time-stamp values. In WebStation, you can create a trend log from a value or from a property in an object.
The EcoStruxure Building Operation software gives you a number of functions to monitor and manage your facilities.