earth_america
user_standard Log on
action_search_stroke
earth_america

AO-8

Refine your search
arrow2_down
Refine your search
Ok
Ok
Ok

34 Topic(s)

Concept

The override switches on Central IO modules with manufacturing date earlier than 2021-W26 must be disabled to remove the risk of an improper output. To disable the override switches, update the Central IO module firmware to version 2.017 or later.

User Interface

The Status LED on the front of the automation devices changes color and flashes to indicate the status of the device.

Concept

There are many different kinds of external devices from different vendors that can be connected to an EcoStruxure BMS.

Concept

The AS-P server offers enhanced processor performance, increased memory size, dual Ethernet ports, and high-speed USB interfaces. The AS-P server is a Schneider Electric manufactured embedded device that generally serves as the lowest tier EcoStruxure BMS server within the EcoStruxure BMS. The AS-P controls and supervises equipment, typically HVAC equipment. AS-P servers use Central IO module with connected field devices, such as sensors and actuators, to do that.

Concept

The Schneider Electric SpaceLogic hardware devices for the EcoStruxure BMS include terminal bases, PS-24V power supplies, Central IO modules, automation servers such as AS-P servers and AS-B servers, BACnet/IP devices such as MP-C controllers, MP-V controllers, IP-IO modules, and RP-C controllers, RP controller expansion modules, remote control, KNX Modbus gateway, Bluetooth adapter, Wireless Adapter - Advanced, SpaceLogic Sensor devices, Advanced Display devices, and Operator Display devices.

Concept

It is important to perform the grounding correctly for the following reasons:

Concept

For Central IO modules with outputs, the following components on the front provide control of the output channels:

Concept

By adding a variety of Central IO and power supply modules, you can use the AS-P server to tailor the Intelligent Building Management System to your unique requirements.

Concept

The AO-8 and AO-8-H Central IO modules are analog output, 8-channel I/O modules.

User Interface

The Central IO modules have the following status indicator LEDs on the front of the module: