earth_america
user_standard Log on
action_search_stroke
earth_america

SpaceLogic Sensor

Refine your search
arrow2_down
Refine your search
Ok
Ok
Ok

52 Topic(s)

Concept

The RP-C sensor bus allows SpaceLogic Sensor devices to be connected to the controller.

Concept

The MP controller sensor bus allows SpaceLogic Sensor devices to be connected to the controller.

Concept

The Schneider Electric SpaceLogic hardware devices for the EcoStruxure BMS include terminal bases, PS-24V power supplies, Central IO modules, automation servers such as AS-P servers and AS-B servers, BACnet/IP devices such as MP-C controllers, MP-V controllers, IP-IO modules, and RP-C controllers, RP controller expansion modules, remote control, KNX Modbus gateway, Bluetooth adapter, Wireless Adapter - Advanced, SpaceLogic Sensor devices, Advanced Display devices, and Operator Display devices.

Concept

SpaceLogic Sensor devices are modular and are ordered in two parts: the sensor base and the cover. Four SpaceLogic communicating sensor base models are available as well as a variety of covers.

Concept

The SpaceLogic Bluetooth Adapter is plugged into a SpaceLogic Sensor to provide a wireless Bluetooth connection to the BACnet/IP controller (Sensor Bus compliant controller) for commissioning, maintenance, and troubleshooting of the controller and the sensor.

How to

You connect SpaceLogic Sensor devices to an RP-C controller to provide the devices with power and communication from the controller.

Hardware Installation

How to

You connect SpaceLogic Sensor devices to an MP controller to provide the sensor devices with power and communication from the controller.

Concept

SpaceLogic Sensors are a family of living space sensors designed for BACnet/IP controllers using the EcoStruxure Building Operation user interface. These sensors use an RJ-45 sensor bus that provides communication and power from the BACnet/IP controller.

How to

The SpaceLogic Bluetooth Adapter allows you to establish a Bluetooth connection to MP and RP controllers. To connect to a device through the SpaceLogic Bluetooth Adapter, a SpaceLogic Sensor must be wired to the controller.