earth_america
user_standard Log on
action_search_stroke
earth_america

AD v2

Refine your search
arrow2_down
Refine your search
Ok
Ok
Ok

9 Topic(s)

Concept

The Schneider Electric SpaceLogic hardware devices for the EcoStruxure BMS include terminal bases, PS-24V power supplies, Central IO modules, automation servers such as AS-P servers and AS-B servers, BACnet/IP devices such as MP-C controllers, MP-V controllers, IP-IO modules, and RP-C controllers, RP controller expansion modules, remote control, KNX Modbus gateway, Bluetooth adapter, Wireless Adapter - Advanced, SpaceLogic Sensor devices, Advanced Display devices, and Operator Display devices.

Concept

AD v2 uses a wired (USB) connection to communicate with EcoStruxure BMS servers. During installation and commissioning, you can use a wireless access point to establish communication between AD v2 and EcoStruxure BMS servers. AD v2 can be powered either by a AS-P server, AS-B server, or USB power adapter.

Concept

You use interfaces to set up, manage and operate the EcoStruxure BMS on a daily basis.

How to

You connect an Advanced Display to a AS-P server or AS-B server in order to communicate with EcoStruxure BMS servers over a USB connection, to supply the Advanced Display with power, and to ensure that its battery is charged.

How to

You install the AD v2 protective frame with its base on a control cabinet to use AD v2 for locally accessing the automation servers. You attach the base on the cabinet using the dedicated holes in the base.

How to

You install the AD v2 protective frame with its base on a wall to use AD v2 for accessing the automation servers. You attach the base on the wall and to the electrical box using the dedicated holes and hole patterns in the base.

How to

You install the AD v2 tablet and the frame on the base to install AD v2 on a control cabinet or a wall and to provide the tablet with a protective frame.

Concept

AD v2 is the successor to AD v1, and offers several improvements such as higher display resolution, enhanced processor performance, and increased memory size. Like AD v1, AD v2 provides a Human Machine Interface (HMI) for local access to the EcoStruxure BMS servers.

How to

You connect Advanced Display to a USB power adapter in order to supply Advanced Display with power and to ensure that its battery is charged.