earth_america
user_standard Log on
action_search_stroke
earth_america

AS-B

Refine your search
arrow2_down
Refine your search
Ok
Ok
Ok

994 Topic(s)

How to

You duplicate a SmartStruxure server from a backup set using Restore when you want to reuse configuration data from a backup set in a standalone SmartStruxure server device.

How to

You manually adjust the SmartStruxure server device clock when you configure or commission a SmartStruxure server device. When the SmartStruxure server device is running on a fully commissioned site it is important that you use a network time server to avoid drifting time in the SmartStruxure server device.

User Interface

The Status LED on the front of the SmartStruxure devices changes color and flashes to indicate the status of the device.

User Interface

Use the Import project dialog box to choose the name of the project you are importing, and to decide if the project is a new one or a replacement for an existing one.

How to

You can use a service_blacklist to direct the EcoStruxure BMS server to send ReadProperty requests, rather than ReadPropertyMultiple requests. They are used to request multiple attributes of different objects with a single request.

Concept

​Values in Building Operation are stored in the Building Operation database with all input decimals. If a stored value consists of more decimals than the operating system is defined to display, the value is rounded off according to the operating system settings before it is displayed in WorkStation.

Hardware Installation

Specifications

How to

You configure an alarm decoration rule to change the properties that are overridden.

How to

You configure the properties of an enumeration alarm to meet the unique needs of your site.