4 Topic(s)
You delete a binding to remove information transfer between two Function Block objects.
Two compatible ports can be connected by a binding. Bindings connect the input port of one Function Block object to the output port of another Function Block object.
Use the Binding Styles submenu to design a clear visual structure of bindings between Function Block objects.
Expression blocks contain expressions deciding upon their behavior. There are three different types of expression blocks: Binary, Integer and Real.