53 Topic(s)
For I/O modules with outputs, the following components on the front provide control of the output channels:
You can wire a terminal base prior to installing an electronics module.
AS-P is the successor to Automation Server, and offers several improvements such as enhanced processor performance, increased memory size, dual Ethernet ports, and high speed USB interfaces. Like the Automation Server, AS-P is a Schneider Electric manufactured embedded device that generally serves as the lowest tier SmartStruxure server within the SmartStruxure solution. The SmartStruxure server device controls and supervises equipment, typically HVAC equipment. AS-P uses I/O modules with connected field devices, such as sensors and actuators, to do that.
You install a terminal base on a horizontal DIN-rail prior to connecting it to its neighboring terminal bases.
The devices are designed mainly for installing on DIN rails in a cabinet.
You install an electronics module directly onto the relevant terminal base, where it will connect to the power supply and address bus.
You connect terminal bases together to provide continuity of the power supply and the address bus.