64 Topic(s)
Demo licenses are used for demonstration purposes, training, or when building a site.
Demo licenses for EcoStruxure Building Operation software are local, bound to the computer, and cannot be shared.
You activate EcoStruxure Building Operation demo licenses for demonstration, training, or when building a site.
You remove demo licenses after they have expired or when you commission a site.
There are a number of different clients, servers, and features that requires licenses to operate.
The EcoStruxure Building Operation software is available for all to download and install. However, you need valid licenses to use the software. The number of users of the software is limited to the number of licenses owned by the customer.
Use the Licenses view toolbar to activate, remove, or repair licenses on the License Server.
All licenses bought from a Schneider Electric vendor are delivered in an entitlement. The entitlements specify the products and features you are allowed to use.
Use the Licenses view columns to view information about activated licenses.