225 Topic(s)
You perform a text search in Building Operation Help to get help on a specific topic.
Use the Search submenu to search in Building Operation, open or search in Help, or check the version of WebStation.
You click Help to get help on a specific topic.
You can display the trend logs as trend log series in a trend chart in a number of ways. For example, you can change the color and weight of the trend log line, or display markers at the time where the trend log value was sampled.
The x-axis of the trend chart represents time. The time span of the axis can be set with a fixed start and end time or with an end time relative to the present time. The axis can be quick-scaled to show the last hour, last day, last month, or last year.
You recheck alarms to refresh the information in the Alarms pane.
You configure WebStation to run in kiosk mode when you want the user to access only a single object in your system, without any toolbars.
Use the Xenta Schedule workspace to navigate, add, remove, or edit events.
You edit the end time for a schedule event to make the event end at another point of time in the schedule. You can edit the end time for weekly events as well as exception events.
You view schedule events to see the schedule for one or more events.