earth_america
user_standard Log on
action_search_stroke
earth_america
Log on to rate and give feedback 1 2 3 4 5 Log on to rate
0
User Interface

User Interface


Products: Automation Server
Functionalities: Hardware
Product version: 1.3, 1.4, 1.5, 1.6, 1.7, 1.8, 1.9
1/29/2018

Automation Server LEDs

arrow1_rotationStatus LED arrow1_rotationRS-485 LEDs arrow1_rotationEthernet LED arrow1_rotationLON LEDs

There are eight LEDs on the front panel of the Automation Server.

 
action_zoom_plus_stroke Automation Server LEDs

Automation Server LEDs

Table: The Eight LEDs

Function

Color

RS-485 A, Tx

Yellow

RS-485 A, Rx

Green

RS-485 B, Tx

Yellow

RS-485 B, Rx

Green

Ethernet, Link/Act/Speed

Green/Yellow

LON, Tx

Yellow

LON, Mode

Red

Status (Automation Server)

Green/Red

Note:
  • The Automation Server Ethernet and Status indicators comprise two LEDs (green/yellow and green/red respectively) in one structure. Normally, when one LED is lit, the other is not lit and vice versa, that is, the indicator will show one color at a time.

The LEDs indicate status of the Automation Server and the ongoing communication.

Status LED

The Status LED on the front of the SmartStruxure devices changes color and flashes to indicate the status of the device.

For more information, see Status LEDs .

RS-485 LEDs

The RS-485 (COM A and COM B) LEDs indicate the condition of the RS-485 communication according to the following table.

Table: RS-485 LED Patterns

LED Patterns

Condition

Yellow, flashing (Tx)

Transmit data

Green, flashing (Rx)

Receive data

Ethernet LED

The Ethernet LED indicates the condition of the Ethernet communication according to the following table.

Table: Ethernet LED Patterns

LED Patterns

Condition

Green, flashing

10 Mbit communication

Yellow, flashing

100 Mbit communication

LON LEDs

The LON LEDs indicate the condition of the LonWorks RS-485 communication according to the following table.

Table: LON LED Patterns

LED Patterns

Condition

Yellow, flashing (Tx)

LON communication RS-485

Red, short flash (MODE)

During start-up; otherwise for future use

  • Automation Servers
  • Status LEDs