The Status LED on the front of the SmartStruxure devices changes color and flashes to indicate the status of the device.
Location of the Status LED on different SmartStruxure device models
The remaining LEDs on the front differ in number and meaning for the different devices and are explained in the sections about the specific device.
The SmartStruxure server device Status LED indicates the condition of the device according to the following table.
LED Patterns |
Condition |
Green, constant |
Normal operation, status OK |
Green, flashing (~1 Hz) |
Device restarting, wait |
Red, constant |
Fatal error - attention required |
Red, flashing (~1 Hz) |
Device operates, but a problem needs attention |
Red/green, flashing (~1 Hz) |
Firmware being downloaded, wait |
Red/green, vague |
Device firmware upgrade mode, wait |
No light |
No input power |
The I/O module Status LED indicates the condition of the device according to the following table.
LED Patterns |
Condition |
Green, constant |
Online and configured (at least one channel/point downloaded successfully) |
Green, flashing (200 ms ON, 200 ms OFF) |
Online and unconfigured (physical module that either matches/mismatches logical module) |
Green, slow flashing (approximately every 3 s) |
Low power mode (saves energy) |
Red, constant |
Error requiring attention (for example, the input voltage is too low) |
Red, flashing (100 ms ON, 100 ms OFF) |
Offline with respect to the SmartStruxure server device (both configured and unconfigured modules) |
Red/Green, flashing (green 100 ms, red 100 ms) |
Bootloader mode (downloading data) |
No light |
No input power |
The PS-24V power supply Status LED indicates the condition of the device according to the following table.
LED Patterns |
Condition |
Green, constant |
Output voltage and load OK |
Red/green, flashing |
Output slightly overloaded |
Red, constant |
Output overloaded |
No light |
No input power |