earth_america
user_standard Log on
action_search_stroke
earth_america
Log on to rate and give feedback 1 2 3 4 5 Log on to rate
0
User Interface

User Interface


Products: PS-24V
Functionalities: Hardware
Product version: 1.3, 1.4, 1.5, 1.6, 1.7, 1.8, 1.9
6/2/2015

Power Supply PS-24V LEDs

arrow1_rotationMain Power LED arrow1_rotationStatus LED

There are two LEDs on the front panel of the PS-24V. The LEDs indicate status for input and output power.

 
action_zoom_plus_stroke ​PS-24V power supply LEDs

​PS-24V power supply LEDs

Table: Power Supply PS-24V LEDs

Function

Color

Main power

Green

Status

Green/red

Main Power LED

The Main Power LED indicates status for input power. The Main Power LED indicates the condition according to the following table.

Table: Main Power LED Patterns

LED Patterns

Condition

Green, constant

Input power

No light

No input power

Status LED

The Status LED on the front of the SmartStruxure devices changes color and flashes to indicate the status of the device.

For more information, see Status LEDs .

  • PS-24V Power Supplies
  • Status LEDs
  • Power Supply Overload