earth_america
user_standard Log on
action_search_stroke
earth_america
Log on to rate and give feedback 1 2 3 4 5 Log on to rate
0
User Interface

User Interface


Products: Registration Portal
Functionalities: Registration
Product version: 1.5, 1.6, 1.7, 1.8, 1.9
5/23/2018

Systems – Installation Tab

Use the Installation tab to view the system installation information. The Schneider Electric partner or branch user cannot edit information if the system is associated to the end-user.

 
action_zoom_plus_stroke Systems - Installation Tab

Systems - Installation Tab

Table: Systems - Installation Tab

Property

Description

System ID

Displays the System ID of the registered system.

Registration code

Displays the Registration code generated by SmartStruxure Registration Portal after successful offline system registration process.

Site type

Displays whether the site has multiple Enterprise Servers (Multi site) or has single SmartStruxure server (Single site).

Site/building name

Displays the site or building name.

Site company name

Displays the company name.

System transition (if applicable)

Displays the systems that existed before on the site.

System application

Displays the applications to which the system is commissioned for.

Segment/application

Displays the business segments you belong to.

Installation address

Displays the site or building address where the system is installed.

Country 

Displays the country to which site or building belongs.

State/province

Displays the state or province to which site or building belongs.

City

Displays the city to which site or building belongs.

Zip/postal code

Displays the zip/postal code of the region where site is located.

Edit

Click to update the system installation information. The partner or branch user cannot update the system information after the end-user has updated it.

  • Edit Systems – Installation Tab
  • Systems - Partner/Branch Tab
  • Systems – Site Administrator Tab
  • Systems – Communications Tab
  • Systems – Warranty Tab