earth_america
user_standard Log on
action_search_stroke
earth_america
Log on to rate and give feedback 1 2 3 4 5 Log on to rate
0
User Interface

User Interface


Products: Registration Portal
Functionalities: Registration
Product version: 1.5, 1.6, 1.7, 1.8, 1.9
5/23/2018

Edit Systems – Installation Tab

Use the Installation tab to edit the system installation information. The Schneider Electric partner or branch user cannot edit information if the system is associated to the end-user.

 
action_zoom_plus_stroke Systems - Installation tab

Systems - Installation tab

Table: Systems - Installation Tab

Property

Description

Site type 

Select the system type. If there is only one SmartStruxure server installed at the site, select Single site option. If there is more than one Enterprise Server installed at the site, select Multi site option.

Site/building name

Type the site/building name where the system is installed.

Site company name

Type the company name where the system is installed.

System transition (if applicable)

Select the legacy systems that existed on the site before installing Building Operation System.

System application

Select the applications to which the system is commissioned for.

Segment/application

Select the business segments you belong to.

Installation address

Type the site/building address where the system is installed.

Country  

Type the country to which site/building belongs.

State/province

Type the state/province to which site/building belongs.

City

Type the city to which site/building belongs.

Zip/postal code

Type the zip/postal code of the region where site is located.

Submit

Click to update the system installation information.

Cancel

Click to leave this page without making any changes.

  • Systems – Installation Tab
  • Systems – Warranty Tab
  • Systems – Site Administrator Tab
  • Systems - Partner/Branch Tab
  • Systems – Communications Tab