earth_america
user_standard Log on
action_search_stroke
earth_america
Log on to rate and give feedback 1 2 3 4 5 Log on to rate
0
How to

How to


Products: Registration Portal
Functionalities: Registration
Product version: 1.5, 1.6, 1.7, 1.8, 1.9
10/2/2015

Editing an Already Registered System

You can update your system information after the system has been registered. For example, if the partner or branch user has already registered the system, the end-user of the system can update the system information before submitting it. The partner or branch user cannot update the system information after the end-user has updated it.

Show More
action_close

You register a Building Operation system offline when WorkStation is not connected to the Internet. When you register offline, you need the system identifier from WorkStation. You then access the Registration Portal on a computer that has Internet access.

You can register at any time in WorkStation by clicking Help > Registration .

To confirm the system registration, the end-user must provide consent for sharing system information and personal information.

For more information, see Providing Your Consent on Sharing System Information .

For more information, see Providing Your Consent on Sharing Personal Information  .

Important:

Each stand-alone SmartStruxure server device is considered as a new registration and a new Registration Code is generated. If a stand-alone SmartStruxure server device is then attached to the Enterprise Server, the SmartStruxure server device’s registration information is overwritten by the Enterprise Server’s registration information.

If the stand-alone SmartStruxure server device is to be attached to the Enterprise Server later, it is recommended not to register the SmartStruxure server device.

Note:

Only the Schneider Electric partner or the branch user can edit the warranty information of the system. The end-user can edit the system information but not the warranty information.

To edit already registered system
  1. Log on to SmartStruxure Solution Registration Portal.

  2. Enter the System ID in Register or Modify a system option and click green arrow.

     
    action_zoom_plus_stroke
  3. Proceed or cancel modifying the system:

    • Click Proceed to register the system if you are the authorized user.

    • Click Cancel to stop registering the system if you are not the authorized user.

     
    action_zoom_plus_stroke
  4. Click Edit .

     
    action_zoom_plus_stroke
  5. Click Submit .

     
    action_zoom_plus_stroke
  • Offline Registration
  • Register Page
  • Systems – Site Administrator Tab
  • Systems – Installation Tab
  • Systems - Partner/Branch Tab
  • Systems – Warranty Tab
  • Systems – Communications Tab
  • Editing System Warranty Information
  • Editing Site Administrator Information
  • Editing Account Information
  • Editing Communications Setting
  • Editing System Installation Information