earth_america
user_standard Log on
action_search_stroke
earth_america
Log on to rate and give feedback 1 2 3 4 5 Log on to rate
0
Concept

Concept


Products: Automation Server, AS-B, Enterprise Server, AS-P, WorkStation, Project Configuration Tool
Functionalities: User Management
Product version: 1.9
5/24/2018

Path Permissions Example

A user account group has the full set of path permissions to the Enterprise Server and no permissions to the Servers folder on the Enterprise Server. A single user account has the full set of path permissions to Automation Server 1, but no path permission to Automation Servers 2 and 3. Even though the user account group has no path permission to the Servers folder, it is possible to give individual user accounts access to individual Automation Servers in the Servers folder.

The path permission rules rely on the actual path string with the name of the SmartStruxure server or folder. If you change the name of a SmartStruxure server or folder, users that earlier had permission are denied access. For example, a user group has full access to the folder LABB. The folder is renamed to Laboratory B. The users that had access to the LABB folder do not have access to the Laboratory B folder or its subfolders.

Note:

The local admin account is always granted access on the local SmartStruxure server. For more information, see Administration Accounts in SmartStruxure Server Local Domain .

 
action_zoom_plus_stroke If you change the name of server or folder, you also have to configure the path permission to the folder.

If you change the name of server or folder, you also have to configure the path permission to the folder.

The System folder and its subfolders, except the Domains folder, are always accessible to a user even when no permissions are configured for the folders. This means that a user can always at least navigate and view the objects in the System folder and its subfolders.

Note:

The Domains folder is the only folder within the System folder with no access for users with no path permissions.

 
action_zoom_plus_stroke The Domains folder is the only folder of the System folder that can be restricted by the path permission.

The Domains folder is the only folder of the System folder that can be restricted by the path permission.

  • Path Permissions
  • Administration Accounts in SmartStruxure Server Local Domain