Use the Event View settings submenu to change the way events are presented.
Event View settings submenu
Command |
Description |
Edit event filter |
Click to open the Select conditions dialog box where you sort the information in the Events pane or an Event View. For more information, see Select Conditions Dialog Box . |
Save as standard layout |
Click to save the current Events pane or Event View layout as the standard layout for all users and for the Events pane or the specific Event View. |
Reset standard layout to factory default |
Click to reset the Events pane or Event View standard layout to factory default. |
Add/Remove columns |
Click to open the Add/Remove columns dialog box to add or remove columns from the Events pane or Event View. For more information, see Add/Remove Columns Dialog Box (Events) . |
Properties |
Click to open the Event View dialog box to view and edit the properties of the Events pane or Event View. For more information, see Event View Properties . |
Edit the style of associated events |
Click to open the Event Styles dialog box where you edit the style of a certain event. For more information, see Event Styles Dialog Box . |
D etail view |
Click to open a detail view for the selected event. For more information, see Alarm and Event Detail View . |