Use the General tab to edit the properties that control how all the trend log series are presented in a multi trend log list.
Changes made on the General tab override settings made on individual series on the Series tab.
General tab
Property |
Description |
Log space (records) |
Select the maximum number of records to display in the list. |
Time zone |
Select the time zone in which the log records are presented. |
Calculation method |
Select a calculation method. For more information, see Calculation Methods . |
Delta over period |
Select True to apply a period to the delta calculation method. For more information, see Calculation Methods . |
Period |
Select the time span for which the calculation method is to be executed. |
Custom period |
Enter a custom time span for which the calculation method is to be executed. |
Custom period alignment |
Enter the time when you want the custom period to start. |