Use the Configure Email page to configure the email properties of the notification.
Configure Email page
Component |
Description |
Subject |
Type the subject text or the substitution code for the subject text the email notification is to have when sent. |
To users and groups |
Click the browse button to open the Users and Groups dialog box where you select the Building Operation users or user groups to whom the email notification is to be sent. For more information, see Users and Groups Dialog Box . |
To email address |
Type the email address of an alternative recipient. |