earth_america
user_standard Log on
action_search_stroke
earth_america
Log on to rate and give feedback 1 2 3 4 5 Log on to rate
1
User Interface

User Interface


Products: Automation Server, AS-B, Enterprise Server, AS-P, Virtual Project Servers
Functionalities: Alarms
Product version: 1.9
12/14/2016

Create Notification Wizard - Configure Write to File Page

Use the Configure Write to File page to configure the write to file properties of the notification.

 
action_zoom_plus_stroke Configure Write to File page
Figure: Configure Write to File page

Table: Configure Write to File Page

Component

Description

File name

Type a name for the file.

Uniquenes s

Select whether to append or prepend a timestamp to the file name, or generate the file without any timestamp.

Overwrite

Select True to overwrite the file when a new file is generated.

  • Notification Distribution Methods
  • Creating an Alarm Triggered Notification
  • Configuring an Alarm Triggered Notification 
  • Creating a Variable Triggered Notification
  • Configuring a Variable Triggered Notification
  • Alarm Triggered Notification View
  • Variable Triggered Notification View