Use the I/O Configuration screen to locally configure inputs and outputs, to go to the About screen or Status screen, and to exit the configuration mode.
I/O configuration screen
Component |
Description |
IO Configuration |
Select to locally configure inputs and outputs. |
About |
Select to go to the About screen. For more information, see About Screen on AS-B Servers . For more information, see About Screen on MP-C or IP-IO Module . |
Status |
Select to go to the Status screen (on AS-B servers). For more information, see Status Screen on AS-B Servers . |
Exit |
Select to exit the configuration mode and return to the Home screen. |