Use the Home screen to get information on the MP-C or IP-IO module model name, BACnet ID, and TCP/IP configuration settings.
Home screen on MP-C or IP-IO module
Component |
Description |
[Model name] |
Displays the MP-C or IP-IO module model name. |
BACnet ID: [BACnet ID] |
Displays the MP-C or IP-IO module BACnet ID. |
IP Assign: [Assignment method] |
Displays the IP address assignment method used for assigning an IP address to the MP-C or IP-IO module. For more information, see IP Address Assignment for BACnet/IP Controllers . |
IP: [IP address] |
Displays the MP-C or IP-IO module IP address. |
SM: [Subnet mask] |
Displays the subnet mask, which is used to determine what subnet the MP-C or IP-IO module belongs to. |
GW: [Default gateway] |
Displays the default gateway (router) address. |
MAC: [MAC address] |
Displays the MP-C or IP-IO module MAC address. |