earth_america
user_standard Log on
action_search_stroke
earth_america
Log on to rate and give feedback 1 2 3 4 5 Log on to rate
0
Concept

Concept


Products: Commission, MP-C, MP-V
Functionalities: Engineering
Product version: 2.0, 2.1, 3.0, 3.1, 3.2, 3.3, 2022
6/5/2018

Electrician Workflow for the eCommission Application

Use this workflow with the eCommission SmartX Controllers mobile application to check out I/O following the installation and wiring of MP Series controllers and other devices. Complete the tasks listed in the following flowchart. Information related to each task can be found in the sections following the flowchart.

 
action_zoom_plus_stroke eComission Application Electrician Workflow

eComission Application Electrician Workflow

Physically wire controllers and other devices

Physically wire together the MP Series controllers and other devices that are to be connected.

Connect eCommission application to controllers

Connect the eCommission application to the MP Series controllers.

For more information, see Connection and Architecture Options .

Start eCommission application and discover controllers

Start the eCommission application and log in, and then discover MP Series controllers on the network.

For more information, see Downloading and Starting the eCommission SmartX Controllers Mobile Application .

Perform I/O checkout of each controller

For each MP Series controller, perform checkout of its inputs and outputs.

For more information, see Performing I/O Checkout .

Continue to other tasks

After connecting and checking out the MP Series controllers, you can proceed to other tasks as needed:

  • Connection and Architecture Options
  • Downloading and Starting the eCommission SmartX Controllers Mobile Application
  • Performing I/O Checkout
  • Capturing a Device with the Controller List Creator
  • Connection Workflow for the Commission Mobile Application
  • Technician Workflows for eCommission Application
  • Flow Balancer Workflow