Use this workflow to connect the Commission mobile application to BACnet/IP controllers.
Related information can be found in the sections that follow the flowchart.
Download, install, and log on to the Commission mobile application, and then accept the Terms of use agreement.
For more information, see Logging on to the Commission Mobile Application .
Power up the BACnet/IP controllers.
For more information, see Powering Up MP-C .
For more information, see Powering Up MP-V .
Prepare a wired or wireless connection for use with the Commission mobile application mobile device.
Connection Type |
More Information |
Wired connection to a single controller |
For more information, see Connecting to Single BACnet/IP Controller by Wire . |
Wired connection to a network of controllers |
For more information, see Connecting to Network of BACnet/IP Controllers by Wire . |
Wireless connection to a network of controllers via a WiFi router |
For more information, see Connecting to Network of BACnet/IP Controllers through WiFi Router . |
Wireless connection to a network of controllers via a wireless access point |
For more information, see Connecting to Network of BACnet/IP Controllers through a Wireless Access Point . |
Start the Commission mobile application and then discover the BACnet/IP controllers on the network.
For more information, see Logging on to the Commission Mobile Application .