Use the Device Restart function to perform a device restart of the BACnet/IP controller.
In the Device List view, select the BACnet/IP controller you want to restart and select Next .
From the Device Settings menu, select Device Restart .
In the Device Restart page, select the type of restart you want to perform. For more information, see Restarting a BACnet/IP Controller .
You cannot perform a restart with a controller that is hosted.
Select Restart .
A Warning window appears. Select Ok .
The controller is restarted and its functionality is restored.