earth_america
user_standard Log on
action_search_stroke
earth_america
Log on to rate and give feedback 1 2 3 4 5 Log on to rate
0
User Interface

User Interface


Products: WebStation
Functionalities: Basic Functionality
Product version: 2022
12/17/2021

Select Dashboard Widgets Dialog Box

Use the Select Dashboard Widget s dialog box to add widgets, graphics, and hyperlinks to a dashboard.

 
action_zoom_plus_stroke Select dashboard widgets dialog box

Select dashboard widgets dialog box

Table: Select Dashboard Widgets Dialog Box

Component

Description

Quick filter

Enter a word or a character to filter on. For more information, see Quick Filter .

Widgets

Click on the widget you want to add to the dashboard.

Browse

Click to browse to add a hyperlink or a graphic to the dashboard. For more information, see Graphics in Dashboards .

Graphics

Click to add a custom type graphic to the dashboard. For more information, see Graphics in Dashboards .

  • Dashboard Widgets
  • Graphics in Dashboards