You use Quick filter to filter out the objects by their names from the list. You can either type the name in the Quick filter box or drag an item from a column in the Alarms pane, the Events pane, an Alarm view, or an Event view and drop it in the Quick filter box.
For example, if you want to find all objects that are named “temperature”, just type “temp” in the Quick filter box and only objects named temperature are displayed in the list.
Filtering on characters in all visible columns
The Quick filter filters on everything that is visible in the columns of the view. For example, if you filter on “20” you do not get any hits. But if you add the column Value, you get hits on the temperature, which is 20, and the setpoint which is 20.
The Quick filter for the Event View filters on records that have already been retrieved from the server.
Quick filter filters on all visible columns in the view
Quick filter is used in the following components in WorkStation:
List View
Alarms pane
Alarm Views
Events pane
Event Views
Alarm or Event details views
Watch pane
Watch Views
Add/Remove columns dialog box
Create object wizard
The Quick filter is used in many components, such as the List View (upper left), the Watch pane (bottom left), and the Add/Remove dialog box (upper right).