Use the Add/Remove Columns dialog box to add or remove columns from the view of objects, such as folders, in the System Tree pane. Depending on the object you have selected in the System Tree pane, you get a different set of column options.
Ad/Remove Columns dialog box