The RP controller expansion multi-sensor can be installed on a dropped (suspended) ceiling, a drywall ceiling, or a junction (gang) box.
Rules and Regulations
The multi-sensor must be professionally installed to comply with the following rules and regulations:
Part 15 of the Federal Communications Commission (FCC) rules
Innovation, Science and Economic Development Canada (ISED) licence-exempt Radio Standards Specifications (RSSs)
2014/53/EU Radio Equipment Directive (RED) of the European Union (EU).
S.I. 2017/1206 - Radio Equipment Regulations 2017 of the United Kingdom (UK)
For more information, see RP Controller Expansion Multi-sensor Regulatory Compliance and Approvals
.
General Installation Requirements
Horizontal installation in a ceiling
The multi-sensor is designed to be installed horizontally in a ceiling. The device can also be installed on a junction box when there is no ceiling and space is opened to plenum.
The multi-sensor must be installed with the passive infrared (PIR) sensor facing down. Installing the multi-sensor on a wall will reduce the coverage range of the PIR sensor.
Notice
|
REDUCED SENSOR COVERAGE RANGE
Always install the device with the passive infrared (PIR) sensor facing down.
Failure to follow these instructions can result in reduced device performance.
|
Installation Using the Mounting Springs
The multi-sensor is typically installed on a dropped ceiling. For that reason, the multi-sensor is delivered with three flexible mounting brackets (springs) preinstalled on the device. The mounting springs enable quick and easy installation of the multi-sensor on a dropped ceiling. The installation requires a clearance hole with a diameter of 75 to 76 mm (2.95 to 3.00 inches) in the ceiling tile.
action_zoom_plus_stroke
Figure:
Multi-sensor installed on a dropped ceiling
The Multi-sensor (RP-C-EXT-MS-BLE) and Insight-Sensor (RP-C-EXT-IS-BLE) are the same size and have the same cabling. This means an already installed Multi-sensor can easily be replaced with an Insight-Sensor, or vice versa.
Installation Using the Mounting Ring
The multi-sensor also comes with a mounting ring, which enables the following alternative installation methods:
Installation on a junction box
The multi-sensor can be installed on a junction box when there is no ceiling and space is opened to plenum. The installation requires an octagon junction box of size 4.0 inches (102 mm) and a minimum depth of 1.0 inches (25.5 mm).
Note:
The octagon junction box is not included.
action_zoom_plus_stroke
Figure:
Multi-sensor installed on an octagon junction box
Tip:
You can use the two alignment notches on the mounting ring to position the device.
Installation on a drywall ceiling
The mounting ring also makes it possible to install the multi-sensor on a drywall ceiling using an appropriate anchoring system. The installation requires a clearance hole with a diameter of 75 to 76 mm (2.95 to 3.00 inches) and two mounting holes that fit number 6, 8, M3, or M4 screws (with or without anchors) in the drywall ceiling. You can use the 1:1 drill template in the installation sheet, which comes with each multi-sensor, to measure out the location of the holes. You can also use the mounting ring to measure out the holes.
action_zoom_plus_stroke
Figure:
Multi-sensor installed on a drywall ceiling