There is one LED on the front panel of the RP controller expansion Zigbee modules.
Zigbee Modules LED (Example for RP-C-EXT-ZB-DALI)
Function |
Color |
Status |
Red, Green |
The Zigbee modules Status LED indicates the condition of the device.
LED Patterns |
Condition |
Recommended action |
Green, constant |
Normal operation, status OK. Device is online. During the initial device power-up process, the LED shows constant red light. As soon as the device is online, the LED returns to constant green light. |
No action required. |
Red, flashing fast (~5 Hz) |
Factory reset mode. The device is being reset to factory settings. When the factory reset is completed, the LED returns to constant green light. For more information, see Zigbee Modules Reset Button . |
No action required. |