The RP controller expansion Zigbee modules have a Reset button on the front.
Zigbee Modules Reset Button (Example for RP-C-EXT-ZB-DALI)
You can reset the Zigbee modules depending on how long you press the reset button.
Mode |
Description |
Factory reset |
Press and hold the Reset button for 5 seconds. The device is reset to factory settings. During the reset process, the LED shows fast flashing red light. When the reset is completed, the LED returns to constant green light. For more information, see Zigbee Modules LED . |